Skip to main content
Visitor II
July 11, 2025
Question

STCS1A

  • July 11, 2025
  • 1 reply
  • 155 views

Hi I am using STCS1APUR to drive 10LEDS IR, (MTSM5116MT2-BK), circuit below

nmohammad_0-1752242913431.png

current should be 1A as of f/b resistance, enable gets turn on as sson as the STM32 MCU comes up, supplying a 3.3VDC PWM though the MCU

issue:

the voltage drop across the led is only 0.6VDC, and they are dim, when checked the current , its less than 0.04A across the LEDS

when there is no trigger there is a 4VDC deop cmpared to the +VLED(24VDC)

i read the sheep twice and unable to figure out the issue

on time is 250msec

1 reply

Andrew Neil
Super User
July 11, 2025

@nmohammad wrote:

the voltage drop across the led is only 0.6VDC


How do you measure that?

LED forward voltages are normally about 1.6V or more ...

 


@nmohammad wrote:

on time is 250msec


and what is the period?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.