Skip to main content
Associate II
April 8, 2024
Solved

STEVAL-ISV020V1 increase VEOC

  • April 8, 2024
  • 2 replies
  • 1342 views

Hi @Peter BENSCH can you help me how to modify the  STEVAL-ISV020V1 to make the VEOC up to 5.3V?

This topic has been closed for replies.
Best answer by Peter BENSCH

Well, the data sheet, section 6.1 describes how VEOC is set with a voltage divider R4, R5, R6. The same designations of the resistors can also be found in AN4397, where the equations 12...14 in section 4.3.3 only have to be rearranged according to the required resistance (VBG = Bandgap Reference Voltage = typ 1.23V).

Regards
/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
April 8, 2024

Well, the data sheet, section 6.1 describes how VEOC is set with a voltage divider R4, R5, R6. The same designations of the resistors can also be found in AN4397, where the equations 12...14 in section 4.3.3 only have to be rearranged according to the required resistance (VBG = Bandgap Reference Voltage = typ 1.23V).

Regards
/Peter

rsmquAuthor
Associate II
April 8, 2024

Can you share me a schematic diagram to make the VEOC up to 5.3V?

Peter BENSCH
Technical Moderator
April 8, 2024

The schematic for this is identical to a smaller VEOC, only the resistors R4, R5 and R6 have to be adapted. Please read the sections mentioned in the data sheet and AN4397 and try to transform the equations.

Regards
/Peter