Skip to main content
Associate II
June 30, 2024
Question

STEVAL-L99615C: Why I can not discharge my battery?

  • June 30, 2024
  • 1 reply
  • 997 views

Dear ST:

Why I can not discharge my battery? Only Charge into it?

my setting are below:

1、Hardware:CN2 connector:I connect a load(small DC fan,or a resistor)to CH+ CH-;

2、Software:In GUI, I run file ( Current Acquistion Init - CC+CSA.csv),

      Activate fuse, Charge ON, Discharge ON;

but my battery did not discharge at all ?

the attached file is my Demo details, Thanks !

1 reply

jingbosAuthor
Associate II
June 30, 2024

I want to add more information:

I can use GUI to charge my battery , and the current usually 30~50mA;

but I can not use Tera term, there is no current flow in Tera term;

Wish this can help !

jingbosAuthor
Associate II
July 7, 2024

Dear ST:

 Finally ,I found the fuse (ITV4030L2015NR)was broken, that was why I can not charge and discharge my battery !

I short circuit (bypass)the fuse ,and all works well now;

I use a DC24V power source, and my charging current is about 1.2A(1200mA);

hope this can help !