Skip to main content
Associate
February 13, 2026
Solved

STEVAL-STPM801 inductor values ? (L2 and L4)

  • February 13, 2026
  • 1 reply
  • 113 views

Both the BoM and Schematic (in the Data Brief) do not show the part numbers or values for L2 and L4 on the STEVAL-STPM801 ORing circuit.  Which inductors are used on the reference design?   Thank you. 

Best answer by Peter BENSCH

Your question has already been answered directly, but here is a summary for other readers who are also looking for an answer to the same question.:

L2 and L4 are not populated on the eval board and therefore not included in the BOM. They are the inductors for optional low‑pass PI filters.
If a front‑end filter is required, you can choose the PI components for the desired cutoff frequency and impedance; the inductor must be rated for the maximum system current.

Regards
/Peter

 

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
March 5, 2026

Your question has already been answered directly, but here is a summary for other readers who are also looking for an answer to the same question.:

L2 and L4 are not populated on the eval board and therefore not included in the BOM. They are the inductors for optional low‑pass PI filters.
If a front‑end filter is required, you can choose the PI components for the desired cutoff frequency and impedance; the inductor must be rated for the maximum system current.

Regards
/Peter