STGAP2D Interlock
Hello,
I have a problem with STGAP2D and the interlock pin.
If the interlock pin is on GND, SD and Brake are high, INB is high and the INA is high for 1s after this time 10ms low, than again 1s high and again 10ms low and so on.
The output A is only low and the output B is 1s low and the 10ms high.
But in the datasheet is written, if the interlock pin is on GND, INA and INB are high, than the outputs also are high.
Can anyone tell me, what is wrong?
I need this funktion.
Thank you and best regards
Stefan