STGAP2D pin8 N.C. explain?
Hi . I'm using STGAP2D SO-14 IC in custom project with custom board , and in datasheet i see pin8 specified as N.C. (not connected). Pin8 must be left floating for ic to function properly , or can it be connected to nearby pin7 (GND) ? Is this pin internally not connected at all (dummy pin) ,or it's connected internally to something ? i'm using single layer pcb currently with pin8 not connected and ic functions properly,but i would like a clear answer about possibility /prohibition of this pin connection - datasheet doesn't explains that . Thanks in advance .