STM32U585 VCAP capacitor voltage
Hi,
I am using STM32U585 IC. I have a question on VCAP (L10) pin capacitor requirement. In recent datasheet it is mentioned rated voltage of the cap to use >10V. Why is it recommended to use10V rated cap for a maximum of 3V on pin. I have a concern on capacitor package. Can I use 6.3V capacitor part?
Also what is the minimum capacitance requirement? If I take DC bias and tolerance considerations of X7R capacitor, I might get around 3.0uF. Is this acceptable?
https://www.st.com/resource/en/datasheet/stm32u585ai.pdf
(refer p.no 150)