STPMIC1 and ST-Link
Hello,
Since I'm trying to design a relatively simple and mainly small STM32MP157FAD1 board (MPU, DDR3L, eMMC, WiFi+BT, microphone, speaker and display), something like a wearable motherboard, I'd like to ask if it would be possible to power the whole system with just a 3.7V LiPo battery via STPMIC1 and if the output voltage will be automatically adjusted after I just replace the "5V_VIN" with my 3.7V input? Also, if I may ask, how do I then address the VBAT and the backup battery? I try to stick as much as possible to the schematics of the different solutions, but the diversity of their boards (Ethernet, USB, HDMI ports, GPIO extensions, ...) just confuses me. One last question, is there a way to externally program the processor (and other things like DDR or eMMC configuration) to save PCB space?
Thank you very much in advance for any advice.
Sincerely