STSPIN230
Hi,
We are using STPIN230 Motor driver in our application
Our BLDC Motor electrical parameters are:
1) Rotor inductance - 0.11 mH
2) Terminal resistance - 10.7 Ω
Queries we have:
1) In our current design we have STSPIN230 connected to motor as follows( inductor 10uH || ferrite bead in series) with BLDC motor windings. Do we need to connect those inductors? If yes, how the value should be selected?
Is it necessary,?
Do we need Ferrite beads as well?
2) Diodes are connected for Back emf protection
Kindy list the changes to be done for better operation of motor.
Note: Our motor rotates well with this connections.