STWBC86 Disable ping while receiver is still on charger
Hello,
I'm developing a charging solution using the STWBC86 controller - is it possible to disable the reping after a received EPT packet from the receiver device (GUI setting: TX EPT PING DIS EX EPT) only while it detects the presence of a receiving device?
Currently, if reping is disabled, after receiving the EPT packet from the receiver, the transmitter will not reping until being reset or via I2C commands, regardless if the receiver is removed from the charger. The use case here would be for the receiving device to be able to terminate the power transfer and the transmitter wouldn't attempt to restart the power transfer until the receiving device is removed from the charger.