STWLC38 EPP support with QI2 chargers and/or future MPP support
We have integrated the STWLC38 into our wireless power receiver design and are aiming to utilize the full 15W power capability. However, we have encountered an issue when using the latest QI2 (MPP) chargers. Our receiver remains in BPP (5W) mode, and we are unable to achieve EPP (15W) as desired.
Interestingly, when we use an older transmitter development kit (P9242-R, now obsolete), we are able to achieve EPP (15W) without any issues. We are keen to understand why this discrepancy exists with the newer QI2 chargers and how we can resolve it.
Additionally, we prefer to use QI2 chargers in our setup due to the presence of a metal ring that ensures proper alignment. Could you please provide guidance on how we can achieve EPP (15W) with QI2 chargers using the STWLC38?
Furthermore, do you have any plans to support the MPP protocol for the STWLC38 in the future? We have noticed that NXP now supports this protocol with their MWPR1516.
Thank you and best regards,
Olivier