STWLC38 register addresses and saving
Hi all,
I have a board designed using the STWLC38 as the Qi Rx. An ESP32 is the host controller using I2C to configure the STWLC38. The communication works OK and I can set and read various registers.
I have two questions on this configuration:
The STWLC38 datasheet lists the functions of all the various registers but doesn't list the addresses for many of them. Are these available elsewhere?
The STWLC38 is powered from the Qi coil so that I can only read/write when I have a successful pairing. How can I save my custom parameters to RRAM using I2C?
Thanks in advance.