STWLC38 TX mode
Hello,
I am trying to use one pair of STWLC38 in TX and RX mode each. And here are my questions.
1) I could find the firmware for RX in ST website, but not the firmware for TX. Does the RX firmware include TX configuration as well?
2) When I debug this chip in GUI, the initial mode is 'standalone'. I assume that if I put 5V to VOUT, the chip consider itself in the debug mode. However, to use this chip in TX mode, we have to give 5V input to the VOUT, which is the same way for debug mode. So, should I change the mode of the chip to TX all the time after I power the chip?
Thanks for your attention.