Skip to main content
Associate II
July 11, 2025
Solved

STWLC38 VRECT over-voltage clamping resistor

  • July 11, 2025
  • 2 replies
  • 458 views

Hello experts, 

I have a question about how to determine the resistance value.
In STEVAL-WLC38RX circuit schematic, R4 = 200, R5 = 200, R6 = NA.
What is the idea behind the values you set?

The electrical characteristics in the datasheet for STWLC38 state Imax = 0.3[A](*1) when Vrect = 5 to 10[V].
   (*1)Non-repetitive 100 ms rectangular pulse

Are the resistance values based on these ratings?
Or is it set based on an experiment?

For now, I plan to use two of the same resistors as on the evaluation board.
Note that only the BPP will be implemented.
Ryoma_0-1752212439273.png

 

Regards, 
Ryoma

Best answer by Ryoma

Hello Didier, 

I see. 
I would like to know if it is safe to charge in BPP using the same parts as the evaluation board.

From now on, I will ask questions at “Support Home.”
Should I click on the link in the red frame in the figure below to make an inquiry?

Ryoma_0-1753248765832.png

Regards, 
Ryoma

2 replies

Didier HERROUIN
Technical Moderator
July 11, 2025

Hello,

These resistors are part of the Over-Voltage Protections.

Indeed, when the VRECT voltage exceeds the programmed threshold (VOUT + SOVP THRES), the resistors are grounded through internal switch to protect the circuit.

For your next requests, do not hesitate to open a case on st.com (https://www.st.com/content/st_com/en/support/support-home.html#), I will be able to support you directly.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RyomaAuthorBest answer
Associate II
July 23, 2025

Hello Didier, 

I see. 
I would like to know if it is safe to charge in BPP using the same parts as the evaluation board.

From now on, I will ask questions at “Support Home.”
Should I click on the link in the red frame in the figure below to make an inquiry?

Ryoma_0-1753248765832.png

Regards, 
Ryoma

Didier HERROUIN
Technical Moderator
July 23, 2025

Exactly !

Then, you will reach the Online Support website where you can create a new case.

Depending on your region and the product, it will be redirected to the right person in ST.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.