UM2458 Inverter (SPC560P50L3 + L6491D): No Gate Drive on MOSFETs
Hello ST community,
I am working with the STM UM2458 inverter board (5 kW low-voltage, high-current inverter) using the STEVAL-CTM004V1 control board with SPC560P50L3 MCU. I am configuring the system in SPC5Studio, debugging with UDE STK, and using Motor Control Live Monitor for motor testing.
My setup:
-
Supply: DC source (up to 48 V)
-
Gate driver: L6491D (configured as per UM2458 schematic)
-
PWM inputs: HS_IN_PWM and LS_IN_PWM are driven correctly from MCU (checked with oscilloscope)
-
Bootstraps and supply voltages (+12 V, +3.3 V) are present
-
Motor: small BLDC A2212/13T 1000 kV for testing
Problem:
-
No switching observed at GATE_HS, SOURCE_HS, or GATE_HS outputs of the L6491D
-
MOSFETs are tested OK with multimeter (no shorts)
-
In Motor Control Live Monitor, I first saw “Speed feedback error” and sometimes startup errors
-
After enabling open-loop FOC (parameter.h), no error is displayed but the motor does not run and MOSFETs still do not switch
Questions:
-
Why is the L6491D not producing gate drive even though PWM inputs are present?
-
Is there a recommended SPC5Studio configuration file for UM2458?
-
Do I need special settings for bootstrap charging or open-loop startup?
-
Any checklist or reference project for UM2458 with SPC560P50L3?
Thanks in advance for your support.
Best regards,
Jenistan J