Unconventional use of L9826 (erroneously before L9925)
In my project I use a L9826, 6 Outputs are used conventionally 2 outputs are not used.
In the same project I need to have 2 digital inputs (SPI) and I would like to know if I could use the two unused outputs of the L9826 as HCMOS inputs via the Fault status register; would this type of unconventional use be possible? Thanks