Skip to main content
Associate
October 30, 2025
Question

Viper12, AC-DC non isolated Buck converter 5V 60mA

  • October 30, 2025
  • 1 reply
  • 221 views

Hello,

 

I'm considering using Viper12 to 3Phase AC/DC non isolated buck converter 5V 60mA Vout. I found some application notes like AN1357. But is it reliable? Or will it cause problems in long-term operation? Has anyone experienced it before?

 

Thanks,

 

Gökhan

1 reply

Peter BENSCH
Technical Moderator
October 30, 2025

Welcome @MGökhan, to the community!

First, a note: the AN1357 is already obsolete and has long been unavailable online (at least on our website).

Although you did not specify the value of your 3-phase voltage, assuming a voltage of 380V, you will not be able to use a controller with buck technology. The reason for this is that with your low output power of 0.3W, the controller would have to have extremely short switch-on times in order to regulate effectively, which such controllers are not designed for. In addition, in this voltage class, a regulator with a maximum reverse voltage of 1050V, such as VIPER265K, would have to be selected, but this is also not suitable for your application.

In your case, a flyback regulator will work most reliably. On the one hand, it requires a transformer, but on the other hand, it can work without any problems with regulators such as the above-mentioned VIPER265K.

Hope that helps?

Regards
/Peter

MGökhanAuthor
Associate
October 30, 2025

Hi Peter,

Thanks for your answer! You can find the AN1357 attached and the file says that it can work with additional components. 

Peter BENSCH
Technical Moderator
October 31, 2025

You still haven't mentioned what the effective value of your input voltage is or what the maximum value of the rectified 3-phase voltage is. Without this information, I'm assuming 380Vac or 540Vdc.

The outdated AN1357 you uploaded refers to a buck converter with a single-phase mains voltage of max. 265Vac and a larger load. In this configuration, such a non-galvanically isolated design can certainly work. The eDesignSuite from STMicroelectronics can also simulate such single-phase designs – but only for reasonable voltage and load ranges.

If your 3-phase voltage is 380Vac, such a buck converter is not feasible for your very low output voltage of 5V, as I explained earlier.

Regards
/Peter