Visitor II
July 16, 2025
Question
Viper35 waking up issue.
- July 16, 2025
- 1 reply
- 216 views
Hello,
For the past few days, I’ve been trying to operate the VIPer35 quasi-resonant offline high-voltage converter, but I haven't been able to get any output. I attempted to bypass or disconnect the output of the PC817 optocoupler and also tried shorting it—still, no pulses were generated. I also connected the ZCD pin directly to ground and then to VDD in another attempt, but there was still no output. Additionally, I tried powering the VDD directly with 15V and even applied 230V AC through a variac, but no pulses appeared.
I need guidance on how to generate pulses or how to properly trigger the VIPer35 IC.
In the oscilloscope yellow graph is Vds and Blue graph is Vdd