Question
VN9E30F Channel deatils
VN9E30FTR – 6-channel high-side driver with 24-bit SPI interface
Max. DC output current is internally limited to 35A for channels IOUT0, IOUT1, IOUT2, IOUT3, IOUT4, and IOUT5
- Whether this 35A limit is shared across all channels or applies individually to each channel.
- What is the maximum current for each channel
- Conditions applicable when switching the load per channel.
- Can we parallel 2 or 3 channels to get single output.
- If we are not using any channel cant it be disabled / floated ( Is SOCR used for Enabling / disabling the channel )