What is max speed of POWERSTEP01 in steps/sec?
In the STPSIN software, it seems that I am limited to 15609.741 Steps / sec?
(See picture below)
With a 0.9 degree motor (400 steps / revolution)
this limits me to
15609 steps/sec * 1 rev/400 steps * 60 sec/1 minute = 2341 RPM
Is this the maximum speed of the device, because I need to move at 3000 RPM?
Is this for trajectory mode only? Can I move faster if I provide the external step pin?
Is there a fundamental speed limit for step mode?