What is the maximum error of STPM32?
Hello,
in the Datasheet of the STPM32 the accuracy of the active power is 0,1% error over 500:1 dynamic range.
Is this the best case error or the maximum error of the enerqy measurement after calibration?
What does the dynamic range of 5000:1 mean?