Why Minimum 125V DC Supply Voltage for STEVAL- IHM023V3 ?
I have been using the PWD13F60 dual H Bridge IC which is a great device but the EVALPWD13F60 Eval board is limited to 2A_rms even though the IC is good for 8A DC due to thermal limitations of the eval board which is a shame as I really need to get about 4A. So i was hoping to jump on to an STEVAL-IHM023V3 using just two channels but I see it wants a minium 125V DC power line. My current power supply is limited to 120V DC which matches other requirements of my project. I was wondering where the 125VDC minimum requirment comes from on the EVALPWD13F60. I scanned the documentation and nothing obvious jumped out at me. Could I run oin 120V DC ?