AS5047P can connect IHM07M1 using motor control workbench
I have a X-NUCLEO-IHM07M1 and a BLDC motor.
BLDC motor have a encoder AS5047P, ABI interface.
first, I just connect encoder pin:
A to PA10;
B to B3;
I to B10;
secondly, change the speed sensor to quadrature encoder, and generate the code;
i just get a error:
"Main speed sensor is set to the Quadrature Encoder sensor, but the motor doesn't support it"
is X-NUCLEO-IHM07M can not support AS5047P?
this is 5047p infomation: