Assistance Required – Motor Issues with MCSDK 6.41 on STM32F303EVAL
Hello Expert,
I am reaching out regarding some persistent issues I am facing with MCSDK 6.41 on the STM32F303EVAL control board with the STEVAL-IPM-NM2S. I suspect there may be bugs or configuration issues.
Background:
-
I previously purchased two boards, and neither motor ran correctly during initial experiments(external opamp case motor work fine)
-
I have now purchased a fresh STM32F303EVAL board and intend to use the internal op-amps and comparators as before. Using external op-amps allows the motors to run, but with internal op-amps, the motors do not start.
-
I followed previous technical support guidance:
-
Set HTMIN2 = 1 and applied the new configuration.
-
Replaced the file r3_2_f30x_pwm_curr_fdbk.c in project\MCSDK_v6.4.1-Full\MotorControl\MCSDK\MCLib\F3xx\Src\ with the attached version.
-
Reduced the PWM pulse width.
-
Observed Issues:
-
Motor 1 always faults (mostly fault code 32), whereas Motor 2 runs without issue. I have tried more many times to play with parameters, suggested in MCSDK FOC errors, but did not help. then i tried Using MC_AcknowledgeFault in code allows both motors to run.
-
High power draw and noise:
-
The motors run at expected RPMs (target speed is correct), but the power draw is unusually high. I mean same rpm, in external opampm draws less power. two ECM motors on the other hand for comparison from the same supplier typically draw ~26 W, but with MCSDK, it draws ~44 W, and there is noticeable humming/noise.
-
-
RPM limitation:
-
When trying to exceed 3700 RPM, the motors do not reach the target and remain stuck around 3000 RPM.
-
Questions:
-
Why does Motor 1 always fault when using internal op-amps, while Motor 2 runs correctly?
-
Could the high power draw and humming noise indicate a configuration issue, SDK bug, or hardware mismatch?
-
Why are the motors unable to reach the target RPM of 3700, even when configured?
-
Are there known limitations in MCSDK 6.41 related to using internal op-amps or comparators on the F303 evaluation board?
I have attached the MCSDK project code for reference.
I have also attached a video, how I am measuring RPM in code. Please advise on possible solutions, or let me know if additional boards need to be purchased for testing.
Thank you for your guidance and support.