Skip to main content
Visitor II
March 3, 2025
Question

B-G431B-ESC1 can't connect to Motor Profiler

  • March 3, 2025
  • 1 reply
  • 432 views

 

Hey, I have troubles with my B-G431.

Two problems with the B-G431:

MotorProfiler 5.4.8: Measurement of Profile is taking too long, no matter how I change the values.

orka375_0-1741011916269.png

 

MotorProfiler 6.3.2: Can't connect to the Board. It can't even open the port. Does anyone know what the correct BAUD Rate should be?

orka375_1-1741012160722.png

What I already tried:

- Reinstalling MC_SDK in Documents

- Flash the file: ...\Utilities\PC_Software\STMotorPilot\STM32CubeProgrammer\Fw with CubeProgrammer, doesn't help, it still doesn't recognize the board.

Also opening the board in CubeProgrammer with the UART Connection is not possible, only the ST-Link works

orka375_2-1741012315304.png

Thanks

1 reply

GMA
Technical Moderator
March 7, 2025

Hello @orka375,

Generating B-G431 with MC-SDK workbench 6.3.2, used Baudrate is available on the "user Interface" tab.

GMA_0-1741366547065.png

Using the "Discover Board" button on MC Pilot V1.2.12 should work. 

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA