B-G431B-ESC1 Encoder Problem
Hi
I want to make a position control with a B-G431B-ESC1.
I use a motor with an encoder with 1024 PPR.
Motor profiler ended with no problem.
I started a project in motor control workbench Ver. 5.Y.1.21203 setting the encoder in motor settings and in speed sensing.
I tryied to generate the code but i get following errors:
Type Time Motor Id Message
UNK 09:07:29 A0 is used in: Encoder Interface Timer( TIM2 ).CH1, Bus Voltage feedback ADC( ADC1 ).ADC12_IN1
UNK 09:07:29 A1 is used in: Encoder Interface Timer( TIM2 ).CH2, Phase current feedback OPAMP( OP1/OP2/OP3 ).ChU NoInv
Any help?
Thanks