B-G431B-ESC1 / MCSDK Motor Pilot/Profiler Failed Connection
Board: B-G431B-ESC1
OS: Windows 11
Attempting to use the Motor Pilot or Profiler but unable to connect. I know I am connected because ST-Link can read the MCU and I am able to program it. From previous posts it seems to be related to the version of MCSDK so I attempted to use 5.4.8, 6.2.1, 6.2.0, 6.1.0, and 6.3.1. Done the obvious restart computer, board, run as admin.
- Generated Firmware using the MC workbench, ensured Motor Profiler was checked in Application Configuration and uploaded to board
- Double checked to make sure UART was initialized
- Another post said to set build configuration to release, didnt work
Not sure how to diagnose from here
From the Motor Profiler (Any of them)
[INFO] - UART worker: Successfully open port COM6 @ 115200
[INFO] - : try to configure the board'
From the Motor Profiler (Any of them)
[ERROR] - : Failed to discover Board at 1843200 Bauds and 115200 Bauds
[INFO] - : disconnect UART START
[INFO] - : Disconnected from board
[INFO] - : disconnect UART END
More information from the programmer
11:54:11 : ST-LINK SN : 0674FF485051727187183257
11:54:11 : ST-LINK FW : V2J45M30
11:54:11 : Board : B-G431B-ESC1
11:54:11 : Voltage : 3.23V
11:54:11 : SWD freq : 4000 KHz
11:54:11 : Connect mode: Normal
11:54:11 : Reset mode : Software reset
11:54:11 : Device ID : 0x468
11:54:11 : Revision ID : Rev X
11:54:11 : ST-LINK SN : 0674FF485051727187183257
11:54:11 : ST-LINK FW : V2J45M30