Bug in Motor Pilot V0.9.20 from ST MCW 5.Y.4.21553 Rev-up Phases Configuration?
My setup:
NUCLEO-F446RE and STEVAL-IPM15B
"ST Motor Control Workbench" "Power Stage - Current Sensing" settings:
- Shunt resistors value: 0.04 Ohm (also on PCB, but User Manual um-2014-1500-... says 0.08 ohm, another mismatch)
- Amplifying network gain: 2.10
- T-rise: 1500
- T-noise: 2000
These values are in "power_stage_parameters.h" too.
However, Motor Pilot in "Rev-up" tab, "Phases configuration" -> click "Read all", reads as follows:
- RShunt: 0.0050 ohm
- OPAMP Gain: 24
- Vref: 3.3 V
That effectively lowers down current/torque about 30% in rev-up phase.
Is it a bug or a feature? Motor Pilot does not read RShunt and gain values from the firmware?
Thank you.