Can STEVAL-ESC001V1 Drive Low-Voltage (3-6V, 0.5A) Motors?
"Hello,
I am using the STEVAL-ESC001V1 motor controller and I would like to know if it can be used to drive a low-voltage motor (3-6V) with a maximum current of 0.5A. The motor is a small brushless DC motor, and I want to confirm whether this ESC is suitable for such low power requirements.
Will the controller function correctly, or are there any limitations due to the voltage and current mismatch?
Thank you!"