Cannot Remap Pins
Cannot Remap Pins
My design (custom PCB) is based on the B-G431B-ESC1. I'm trying to swap the V and W PWM channels. I cloned the B-G431B-ESC1 board and just swapped the pin definitions for the V and W high and low channels. No errors during generation or build. However, the motor doesn't turn and the CubeMX IOC file has those four pins locked (purple) in reset state. This issue existed in V6.2.1 and I hoped it would be resolved in V6.3.0 but nope. My CubeMX is fully up to date (6.11.1) and I'm using FW 1.5.2 (recommended).

Frustratingly, I can't even choose to swap V and W channels on the current sense side, because I later get an error saying it's not compatible with the FOC algorithm.