Skip to main content
Associate
August 7, 2024
Solved

Connecting STEVAL-SPIN3204 to PC

  • August 7, 2024
  • 2 replies
  • 1131 views

Hi, I recently bought a STEVAL-SPIN3204 and now i want to connect it with my PC, i connected it with the USB cable, selected an example project for this device and clicked on connect, but there comes always the error message, connection failed. What did I do wrong or have i forgotten? Here you can see a picture of the interface:

I also checked the baudrate and everything.

Christian3_0-1723022150283.png

 

Best answer by Gael A

Hello Christian3,

Could you please be more specific with your procedure ? What version of the MCSDK are you using ? Have you considered upgrading to our latest (6.3.0) version ? Which IDE have you used for flashing the code, and which version ?

When you say that you checked the baudrate and everything, could you be more precise ? Are you sure the COM port is the right one ?

2 replies

Gael A
Gael ABest answer
ST Employee
August 8, 2024

Hello Christian3,

Could you please be more specific with your procedure ? What version of the MCSDK are you using ? Have you considered upgrading to our latest (6.3.0) version ? Which IDE have you used for flashing the code, and which version ?

When you say that you checked the baudrate and everything, could you be more precise ? Are you sure the COM port is the right one ?

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.
Associate
October 1, 2024

I wrote you an email!