Skip to main content
RHube.3
Associate
November 30, 2022
Question

Do I need an external clock for a BLDC (FOC) driving circuit or is the internal clock precise enough?

  • November 30, 2022
  • 0 replies
  • 579 views

The STSPIN Eval Boards I checked do not use an external clock source. They all use the internal HSI Clock as source. If I choose a STSPIN Project in the ST Motor Control Workbench, I can choose between internal and external clock. If I choose a single uC, for instance STM32F031C6, I can only select an external clock source.

An external clock source is better for sure, but is it really necessary for a BLDC solution (FOC)? I would say not really, what's your experiences?

This topic has been closed for replies.