Electrical Angle Synchronization in MCSDK v6.4.0 to avoid long-term drift.
Question about Electrical Angle Synchronization in MCSDK v6.4.0
Hi everyone,
I'm using MCSDK v6.4.0 with an STM32G4, a 42BLF01 motor, and a high-quality incremental encoder with Z-index.
My goal is to accurately correct the electrical angle on each Z-pulse to avoid long-term drift after 100 rounds.
In previous SDK versions, there was a function called ENC_SetElAngle() which allowed setting the electrical angle directly.
In MCSDK v6.4.0, however, this function no longer exists – and the corresponding enc_driver.h file is also missing.
Main Question:
Is there any official or recommended way in MCSDK v6.4.0 to directly set or correct the electrical angle at the Z-pulse – without using ENC_SetElAngle()?
If not:
What’s the recommended strategy for drift-free synchronization while the motor is running?
Is MC_SetCtrlPositionAngle1() the intended method – even though it may cause stepping or jitter?
Thanks for any insights