Evspin32G4-dual : Turning 2 motors simultaneously
Hello,
I have an EVSPIN32G4-Dual, I am Trying to Run 2 HooverBoard Motors (36V/15A/510RPM/HALL).
I generated the firmware using Mc Workbench 6.2.1 and desabled the overcurrent protection for stage 2.
Then tried to command the motors using motor pilot, turning each motor separately work fine,
But trying to turn one after the other, the 2 motors start shaking (didn't even start turning) ending up with one of them turning off or both, with an error of Over current in stage 1 and driver protection in stage 2.
Is there anyone used this board and managed to run 2 motors simultaneously.
Thank you in advance.