EVSPIN32G4 Motor Current Sensing
Hello,
Here are a few things I need to clarify regarding the EVSPIN32G4 current measurement and the related MCSDK software:
Referring to section 5.6.1, 5.6.2 and 5.6.3 of the UM2850, I believe that the topology using three standalone OpAmps presented in section 5.6.2 is not currently supported by MCSDK, is this correct?
So, considering the 2 topologies presented in 5.6.1 and 5.6.3, is there a major disadvantage to go for the internal PGA solution compared to the first configuration which requires external feedback networks on the inverting side of the OpAmp?
At the end of section 5.6.3, it is recommended to connect the inverting input of the PGAs to shunt resistors to perform differential current measurement in case of high current application, but I don't have the possibility to do it in MCSDK since only the "single ended" sensing type is available, what do you propose in this case?
Thanks in advance and best regards.