Skip to main content
Associate
October 21, 2025
Solved

Generating project files using ST Motor Control Workbench resulted in an error

  • October 21, 2025
  • 2 replies
  • 350 views

I'm currently encountering an issue with the P-NUCLEO-IHM001 motor. I'm using STM32Cube version 6.10 and X-CUBE-MCSDK version 5.4.8. During file generation, the problem shown in the image has arisen. How should I resolve this?

*This post has been translated from Chinese to comply with the ST Community guidelines.

Best answer by GMA

Hello @Lzj111111,

The language of the Community is English as mentioned here.

Refer to the MCSDK5.4.8 release note for the STM32 environment. You must first install STM32CubeMX v6.4.0 and the expected STM32Cube_FW_F3_V1.11.3 firmware package (in your image, it is mentioned as expected but not installed).

2 replies

GMA
GMABest answer
Technical Moderator
October 21, 2025

Hello @Lzj111111,

The language of the Community is English as mentioned here.

Refer to the MCSDK5.4.8 release note for the STM32 environment. You must first install STM32CubeMX v6.4.0 and the expected STM32Cube_FW_F3_V1.11.3 firmware package (in your image, it is mentioned as expected but not installed).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
Lzj111111Author
Associate
October 21, 2025

After following your instructions, I encountered the error shown in the image. How should I resolve this? Thank you.

*This post has been translated from Chinese to comply with the ST Community guidelines.

GMA
Technical Moderator
October 21, 2025

Hello @Lzj111111,

If the project generation finishes with the generation of the main.c file, proceed with the generated project.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA