Skip to main content
DHemb.1
Associate II
April 12, 2023
Solved

Hall Sensor Connections to J1 on X-NUCLEO-IHM16M1/NUCLEO-G431RB

  • April 12, 2023
  • 5 replies
  • 1990 views

I have a X-NUCLEO-IHM16M1/NUCLEO-G431RB eval board I am trying to connect to a motor with hall sensors. The motor has leads labeled Hu, Hv, and Hw, but J1 on the driver board is labeled A+/H1, B+/H2, Z+/H3. What is the correlation between these two nomenclatures?

Thanks,

Dan

This topic has been closed for replies.
Best answer by Gael A

Hello @DHemb.1 (Community Member)​,

This is a MCSDK 6.1.1 common issue that will be fixed on next release. In the meantime, you can refer to this post to solve your problem.

Hoping it will help,

Gaël A.

5 replies

Gael A
ST Employee
April 13, 2023

Hello @DHemb.1​,

Looking on the IHM16 User Manual here, at section 4.5 Hall effect sensors and encoder connector, you can see that A+ corresponds to Hall 1 (H1), B+ to Hall 2 and Z to Hall 3. This should cope well with your motor's leads labeled Hu, Hv and Hw (A+ on Hu, B+ on Hv and Z to Hw). However, if you are not sure, you can still check your motor's specification for more information on each lead.

Hoping this will help,

Best regards,

Gaël A.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.
cedric H
Technical Moderator
April 13, 2023

Hello @DHemb.1​ ,

In addition to Gael's answer, I would recommend you to test the new Hall sensor profiler feature provided with the profiler tool of the 6.1.1 release. It will help you to determine the Hall sensors placement angle and the shift between the Hall sensors and the electrical angle.

Best regards

Cedric

DHemb.1
DHemb.1Author
Associate II
April 13, 2023

Thanks for the replies.

I was able to verify the connections @Gael A​ suggested, and am currently trying to get the Profiler working. Perhaps this is better moved to a different thread, but the Profiller (V1.1.5) gets hung up trying to connect to the board. Initially it displays a warning stating the Motor Profiler image is needed, and when I select Accept it spins on "Check ST-Link connection". I can communicate with the board via Motor Pilot, so I don't think there is a connection error. I'm very new to this platform so any help is greatly appreciated.

Gael A
Gael ABest answer
ST Employee
April 14, 2023

Hello @DHemb.1 (Community Member)​,

This is a MCSDK 6.1.1 common issue that will be fixed on next release. In the meantime, you can refer to this post to solve your problem.

Hoping it will help,

Gaël A.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.
DHemb.1
DHemb.1Author
Associate II
April 20, 2023

@Gael A​, that link solved the problem, thanks!