Skip to main content
Associate
October 15, 2025
Question

Hardware Design for ACIM Sensorless FOC or V/F (STM32MotorControl Wiki Example)

  • October 15, 2025
  • 1 reply
  • 280 views

Hello ST Community,

I am developing a product for residential pump control based on AC Induction Motor (ACIM). I am using the STM32 Motor Control SDK and have been studying the example on the wiki page: STM32MotorControl: SDK_AC_induction_motor.

This software example is a good starting point. However, for hardware, it references the use of three separate evaluation boards (e.g., STM32 Nucleo, X-NUCLEO-IHM, and a power board). For a real product, this approach is too large and expensive. I am looking for a dedicated, consolidated hardware reference design for this application. Specifically, I need a complete schematic that integrates the STM32 MCU, the 3-phase inverter (with gate driver or STSPIN), current sensing, and power supply onto a single board.

Does ST provide such a dedicated, consolidated reference design for a sensorless FOC ACIM driver? If so, what is the design name or document number?

Are there any existing reference designs (even for PMSM) that I can use as a foundational hardware template and adapt for an ACIM?

Thank you for your time and support.

1 reply

GMA
Technical Moderator
November 3, 2025

Hello @Amirmhz,

The STEVAL-IPM15B power board is targeted for the ACIM example that will be available in the MCSDK6.4.2 version.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA