Skip to main content
KSpeh.1
Associate
March 14, 2022
Solved

Hello, I am working on project with STSPIN32F0, and when compiling example in ST MOTOR CONTROL Workbench (version - X-CUBE-MCSDK_5.Y.4) I get errors which cannot be resolved? See errors in the picture below and log file attached.

  • March 14, 2022
  • 1 reply
  • 706 views
This topic has been closed for replies.
Best answer by TDK

It is possible the framework can't correctly handle a space in the path.

It says it can't delete a file. Go see if you can or if something is holding it open.

1 reply

TDK
TDKBest answer
Super User
March 15, 2022

It is possible the framework can't correctly handle a space in the path.

It says it can't delete a file. Go see if you can or if something is holding it open.

"If you feel a post has answered your question, please click ""Accept as Solution""."