Skip to main content
Associate III
December 3, 2025
Question

How can I configure the board under senseless mode?

  • December 3, 2025
  • 2 replies
  • 134 views

Hello Everybody,

Here are the software and boards in this case:

1. MC workbench 6.3.2
2. STEVAL-IHM039V1/STEVAL-CTM009V1

I have an I-PMSM motor, and I use the board (STEVAL-IHM039V1/STEVAL-CTM009V1) to run the ST Motor Pilot for spinning the motor. However, when I try to use the senseless mode, it always reports an error "Start up failure". Should I make some other configuration in ST Motor Pilot? Thanks!

039V1_senseless_startupFault.jpg 

2 replies

Senior III
December 3, 2025

The starting point is always to verify the documentation for the startup failure reasons. 

GMA
Technical Moderator
December 5, 2025

Hello @DF_MC,

For Error description and management, refer to documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab, "(FOC) Firmware errors" link.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA