Skip to main content
Dense505
Associate
November 28, 2022
Question

How can I set up simple open loop V/F control with the STEVAL-CTM012V1

  • November 28, 2022
  • 0 replies
  • 634 views

I am trying to run a small, three phase induction motor from a single phase supply. The STEVAL-CTM012V1 has more than enough power rating. I have wasted hours trying to get something working. All the files I can download seem to want to do fancy FOC for PM motors.

Can you help me with any code example or app note or other resource for basic induction motor open loop V/F control with the hardware that I have?

I have tried all of the firmware that I can find for the CTM012 eval board but it is only for PM motors with FOC.

I have tried creating projects in MCSDK 5.Y.4 and choosing ACIM but that only seems to work with STM32G4, I selected the Control Unit as STSPIN32F0601 but the generated code was full of references to STM32G4 and I spent hours trying to reconcile those but never got it working.

It seems this should be not so difficult.

I have the hardware, I can program it, I have had the MC_SDK_5.4.8 monitor working with the hardware and reading the DC bus voltage correctly but I cannot make the motor run.

This topic has been closed for replies.