Skip to main content
ABlak.1
Associate III
December 29, 2022
Question

How do I use the Motor Pilot 6.1.0?

  • December 29, 2022
  • 1 reply
  • 723 views

0693W00000Y75RRQAZ.png0693W00000Y75RHQAZ.pngI have a motor running in the V1.1.3 Motor Pilot.

Now what?

I built a 6step controller of a hi-revving, low inductance/resistance motor. It compiled in STM32CubeIDE and is pushed to the board.

I started the motor pilot and successfully connected to the board.

Made a couple of updates to the input a table of ramp up values - see image. Then monitor bemf (on the graph) and start the motor. It runs for several seconds before indicating "start-up failure"

Is there some documentation about how to tune the app and motor? 0693W00000Y75R7QAJ.png 

Also how do I manipulate the graphs? I notice if I use more buffers I can capture more details but can not zoom it.

This topic has been closed for replies.

1 reply

STrzb.1
Visitor II
January 5, 2023

I found 6.1 to be quite different than the previous version. It seems erratic.