How to assign internal pin PE15 as driver protection for custom STSPIN32G4 inverter board?
To clarify the details about my environment:
STMC Board Designer v1.0.0
Motor Control WorkBench v6.3.2
Now to my question:
For the STSPIN32G4 Eval board example, the PE15 Pin is assigned for driver protection trigger input.
This makes sense, because the datasheet of the STSPIN32G4 also indicates PE15 as the internally connected fault timer input pin.

But when I try to create a custom inverter board, I can only select pins that are also available on the package itself.
Since PE15 is only internally connected, I can't select it.

How can I assign the pin in the board specification?
Any help is welcome :)
Best regards,
Daniel