i got a STEVAL-CTM010V1 board and installed the SDK(5.4.4 full),after that i created a project base on example(STEVAL-CTM010V1 dual drive with PFC,see pic_1),but the example does not enable the PFC feature(see pic_2),so if we want to use the PFC feature on CTM010V1 board ,what should we do ?
i found a tips to fix this issue,just need to modify the config.xml file(C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.4.4\Utilities\PC_Software\STMCWB\assets\xml).
hence,if you remove the warning ,you can config the PFC feature on WB.