How to drive the high-side of the bridge in STSPIN32F0?
Hi all,
I am new to motor control, and I am currently working with the BLDC motor driver board STEVAL-SPIN3201 (based on the STSPIN32F0). I am trying to generate the corresponding PWM signals to drive a BLDC motor. Although the low side of the bridge is working, whenever I try to drive the high-side MOSFETs I get a voltage of around 40 mV in the midpoint between the high and low side of the bridge (e.g., OUTU). When looking at the signal through a oscilloscope I get the attached outcome. Does anybody know what the issue could be? Am I missing something in the control logic driver to enable the OPAMPS?
Also, when I disable both output compare signals (OC1E, OC1NE), I get a voltage in OUTU of around 11 V (supply is 24 Vdc). Is this correct?
Hope that everything is clear.