Skip to main content
BTrem.1
Senior
February 25, 2022
Question

How to upgrade an existing project from MotorControl 5.4.4 to 5.Y.4 ?

  • February 25, 2022
  • 0 replies
  • 633 views

I use STM32CubeIDE (1.5.0) as a toolchain without a current CubeMx file. What is the means of upgrading motor drivers from 5.4.4 to 5.Y.4?

I have done the basic install of 5.Y.4 under folder C:\Program Files (x86)\STMicroelectronics but in my CubeIDE project the drivers are duplicated under folder:

C:\Users\Brian\ST_workspaces\Bitbucket - repo -v03.10.02 - New_Filter\cascade_pfd\Prysm_Test_Board_LL

I tried replacing the 5.4.4 folder in my project with the 5.Y.4 folder but get a build error.

0693W00000KachAQAR.jpg 

I then edited the path in Project//Properties/Paths to the new folder location of 5,Y.4..

Are there any notes somewhere to go through the steps of upgrading the motor drivers?

Thanks,

Brian

This topic has been closed for replies.