Question
I will create code for discovery kit 'B-G431-ESC' as described in UM2516 chapter 6.1 step 2 and 3 but I get error when compiling with STM32CubeIDE . Is there a more detailed description for generation or an example for this evakit?
I use MCSDK v5.4.7 and STM32CubeIDE 1.6.1. Project generation with MCSDK is successful but when I try to build code with the IDE it ends with fatal error "sto_cordic_speed_pos_fdbk.h: No such file or directory". Run code generation with an other example project works well. So I asume that my tool chain is okay.