IHM17M1 For Motor profiler can't profile known motor
Hello! I'm trying to configure the following setup to run the motor profiler in order to characterize a set of small/low-power BLDC motors.
Configuration:
I'm using MCWB 6.21
Control board: Nucleo F401RE in the following configuration:
JP5 at U5V,
JP1 OFF,
JP6 ON.
Powerstage IHM17M1:
JP6 and JP5 are bridged (shorted),
JP3 and JP4 are both bridged/shorted from "middle pin to 3sh."
To make sure that the profiler works at all, I am trying to use the Bull Running BR2804-1700kv when configuring the project in the MCWB and start by profiling that motor. The resulting project is very similar to the one generated by the pre-configured package IHM002. After checking the "motor profiler" under application configuration and generating the code, I get very strange behavior from the Motor Profiler.
Problematic Behaviour:
After pressing "start profiling," D13 and D11 on IHM17M1 light up continuously while D12 is off for. The LED's dips in intensity before turning off completely - and then nothing else happens until I get the error "the measurement is taking too time" and the suggestion to change the motor max speed. The motor parameters are not the issue for sure, as the parameters are known. There are no errors generated, which complicates troubleshooting.
I have appended a short video on the what happens as I launch the profiler, perhaps someone has had a similar issue. The video is on youtube: https://youtube.com/shorts/AIXBg86RHH0?feature=share
After edit:
Additionally I've uploaded the stwb6 configuration for reference:
https://drive.google.com/file/d/1AOVDi6sdXMMPho9IscoAqq45YDbdqG65/view?usp=drive_link
Comment:
Also I got the testcode for 6-step example code running for the full setup with a different jumper configuration. So I belive there are no hardware failures, although it could still be as the FOC and 6-step are using slightly different hardware resources on the evaluation board.
Question:
- Does anyone have any suggestions on how I could move forward?
- Is there something regarding compatability for the FOC/motorprofiler that I have missed and that this setup is not supported or similar?
Best regards,
Gustav Eckerbom