Input of Motor Parameters from Data Sheet in STM32 Motor Control Workbench
Hello ST Community,
I am currently working with a motor that isn’t compatible with the motor profiler, so I need to manually input the motor parameters provided in the data sheet.
The data sheet specifies the following values:
- Rs (phase-to-phase) = 16.1 ohms
- Back EMF constant = 0.121 V/Krpm
- Ls (phase-to-phase) = 0.140 mH
To correctly enter these values in the configuration, should I input them as:
- Rs = 16.1 ohm
- Ls = 0.140 mH
- Back EMF constant = 0.121 Vrms/Krpm ?
Or is there a different approach or format I should follow when inputting these parameters?
Thank you in advance for any guidance!