Skip to main content
Associate II
August 20, 2025
Solved

Is DPWM supported on HSO?

  • August 20, 2025
  • 1 reply
  • 269 views

Hello,

I am currently working with HSO for motor control and would like to clarify whether DPWM (Discontinuous PWM, 2-Phase PWM) is supported.

In the Observer + PLL method, it seems possible to select discontinuous PWM by setting the modulation flag.
However, I noticed that such an option does not appear to be available in HSO.

Thank you in advance!

wow_0-1755677231818.png

 

Best answer by FouadB

Hello Wow,

You are absolutely right, the modulation option available in the STO-PLL configuration does not currently appear in the Workbench interface for the HSO case.
This feature is planned to be added in upcoming MCSDK releases.

For testing purposes, it is possible to modify the modulation mode through the register interface using the ST Motor Pilot GUI, as illustrated in the figures below:

Screenshot 2025-08-20 162715.jpg

If this meets your requirements, you can update the default modulation mode directly in the firmware code (mc_config.c) by modifying:

.modulationMode = FOC_MODULATIONMODE_Centered,

to either:
.modulationMode = FOC_MODULATIONMODE_MinLow,

or
.modulationMode = FOC_MODULATIONMODE_MaxHigh,

for your information the supported modulation modes are:
FOC_MODULATIONMODE_Sine
FOC_MODULATIONMODE_Centered
FOC_MODULATIONMODE_ShiftedCenter
FOC_MODULATIONMODE_MinLow
FOC_MODULATIONMODE_MaxHigh
FOC_MODULATIONMODE_UpDown

Regards,

Fouad

1 reply

FouadB
FouadBBest answer
ST Employee
August 20, 2025

Hello Wow,

You are absolutely right, the modulation option available in the STO-PLL configuration does not currently appear in the Workbench interface for the HSO case.
This feature is planned to be added in upcoming MCSDK releases.

For testing purposes, it is possible to modify the modulation mode through the register interface using the ST Motor Pilot GUI, as illustrated in the figures below:

Screenshot 2025-08-20 162715.jpg

If this meets your requirements, you can update the default modulation mode directly in the firmware code (mc_config.c) by modifying:

.modulationMode = FOC_MODULATIONMODE_Centered,

to either:
.modulationMode = FOC_MODULATIONMODE_MinLow,

or
.modulationMode = FOC_MODULATIONMODE_MaxHigh,

for your information the supported modulation modes are:
FOC_MODULATIONMODE_Sine
FOC_MODULATIONMODE_Centered
FOC_MODULATIONMODE_ShiftedCenter
FOC_MODULATIONMODE_MinLow
FOC_MODULATIONMODE_MaxHigh
FOC_MODULATIONMODE_UpDown

Regards,

Fouad

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""
wowAuthor
Associate II
August 21, 2025

Hello Fouad,

 

Thank you very much for your detailed and helpful response.

This will be very useful for our ongoing work with HSO.

Thanks again for your support and for sharing such a clear and comprehensive answer!